How can we help you today?

Is there any common selector switch key used in ZB4BG* and 9001KS**K devices ?

Issue:
Do we offer a 9001KS keyed selector switch with ZBG type of key?

Product Line:
Push Buttons and Operator Interface

Environment:
9001K/SK 30 mm Operators

Cause:
Determine if the same keys can be used on both 22mm and 30mm operators.

Resolution:
Yes, a Ronis 455. The 9001KS devices with the Ronis 455 key are noted by adding an R to the part number after the key withdrawal code. EX 9001KS11K1R.

Schneider Electric Canada
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
Start your sales inquiry online and en expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings