Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Class 8502 Type SCG__ contactor be converted to a 8536 starter by adding 9065SDO__ or 9065SS__ overload relay and 9066SC1 external reset mechanism?
Issue:
Can an overload be added to 8502 Type S contactors to convert it to one starter?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment
NEMA Type S Contactors & Starters

Resolution:
The open style contactor inside can be modified by adding the appropriate overload relay however there are no provisions provided on the enclosure cover for mounting the 9066SC1 external reset mechanism. The solid state overload is only for three phase power systems. While you can add overload relays to the size 00, size 0, and size 1 contactors, you cannot for the size 2 and above.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings