Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which Hand-Off-Auto selector switch is used for field installation on an 8810 two-speed starter?
Issue:
What hand off auto switch should be used as a field install kit for the 8810 two speed starters

Product Line:
8810 Multispeed Magnetic Starters

Environment:
Products sold and used in the United States

Cause:
HOA needed for the 8810 two speed starter, either as a replacement or field install kit

Resolution:
Use the 9001 KS 3-position selector switches. Select according to function desired. There are no ready-made kits available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings