Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a handle tie for the outside two poles of the HOMT quad breaker?
Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
No, there is not a field installable handle tie for the outside poles of an HOMT quad breaker. However, there are HOMT quad breaker available with the outer poles tied.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings