Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the add-on K-line auxiliary contacts mechanically linked ?
Issue:
K/Line auxiliary contacts mechanically linked

Product Line:
IEC contactors and Starters

Environment:
Tesys K

Resolution:
No, they are not mechanically linked. If mechanically linked aux contacts are needed, look at D-line devices

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings