Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the sub feed circuit breaker kit for a 225 ampere NQ panel?
Issue:
What breaker can be used to feed out of a 225A NQ panel above 150A?

Product Line:
LV Panelboards

Environment:
NQ Panelboards

Resolution:
For Powerpact Q frame sub feed breaker (70-225A / 240V) a NQSFB2Q Sub feed Breaker kit can be used . For the Powerpact H and J frame breakers ( H frame 15-150A / J frame 150A-250A / 600V), the NQSFB2HJ Sub feed Breaker kit can be used to sub feed out of the Panel.

Schneider Electric Canada

Attachment(s)
NQ Sub-Feed Circuit Breaker and Adapter Kit Installation 80043-730-01 tri.pdf [7.85 MB]
H and J frame sub feed breaker installation 80043-725-02.pdf [9.12 MB]
Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings