Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an EZMR114125, series M01 branch unit?
Issue:
Repair parts

Product Line:
EZM Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover - EZM114125C (includes labels)
Cover Screws - 4020513002K (bag of 10 screws)
Meter Socket Cover - MMRC
Parts Kit - MM125KIT (one position, meter socket line side through tenant breaker base)
Circuit Breaker RB Cover - BCV (one position)
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772301
Equipment Ground Bar Assembly - 7329897053 (includes 4 lugs)
Mounting Screws for Equipment Ground Bar Assembly - (2) 2142217101
Removable Top Driphood (required for NEMA 3R Installations) - 7329714601
Top Driphood Mounting Screws - 4020513002K (bag of 10 screws; only 2 screws are required)
End Closing Cap Kit - EZMCAP (left side)
End Closing Cap Kit - EZMSCAP (right side)
Top Endwall Rain Cap – 7329714601
Top Endwall Rain Cap Mounting Screws – 4020513002K (includes 10 screws; only 2 screws are used to secure the rain cap)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings