Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the NEMA rating for the S29338 handle for the powerpact H and J frame breakers?
Product Line:
Circuit Breaker Accessories

Resolution:
The handle mechanism can be used in NEMA 3R and 12 enclosure applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings