Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part numbers for a sub feed lug kit main lug NQ panelboard (MLO) ?
Issue:
Sub feed lug kit for main lug NQ panelboard (MLO)

Product Line:
NQ Panelboard

Environment:
Products sold in North America

Resolution:
The part numbers for single phase and 3 phase panelboards NQ panelboards are below
AmpCatalog #Instruction Bulletin
100 ANQSFL180043-729-01
225 ANQSFL280043-729-01
400 ANQSFL480043-745-01
600 AUse Feed Thru Lug Kit

Also the sub feed lugs requires additional box space. See the box requirements for the sub feed lug kits in the below table. The important variables are the number of spaces available in the panel and the amperage of the panel.
Feature Circuits 100 A225 A400 A600 A
18MH26Use FTL
30MH32MH38MH50Use FTL
42MH44MH50Use FTL
72MH50MH62Use FTL
84MH56MH68Use FTL

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings