Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can panelboard boxes such as MH35 or MH50 be extended in a vertical direction top or bottom?
Issue:
MH box extension

Product Line:
Panelboards

Environment:
NQ,NF Panelboards

Cause:
Added Gutter Space

Resolution:
Yes. Vertical wireway extensions are available from 4`` to 60`` in 1`` increments for the MH series boxes. They come with the appropriate length cover. Typical catalog numbers are : WW4 for the 4`` length, WW12 for the 12`` length, etc.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings