How can we help you today?

Can the cover of a M800R or M800S circuit breaker enclosure be padlocked closed?

Issue:
Product Features

Product Line:
CB Enclosure

Resolution:
Yes, the cover on these enclosures can be padlocked closed via a hasp located on the bottom endwall. On the M800R only, there is also an integral circuit breaker access cover that can be padlocked closed.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors