Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are PowerPacT H and J frame breakers DC rated?
Issue:
Do the J-frame and H-frame circuit breakers have a DC rating?

Product Line:
Circuit Breaker

Resolution:
Powerpact H and J frame circuit breakers with thermal/magnetic trip units are DC rated with a maximum DC rating of 250 Vdc (20 kA interrupting rating).

Powerpact H and J frame circuit breakers with electronic trip units are AC rated only.

Besides the above, there are special 500 Vdc Powerpact H and J frame circuit breakers available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings