Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the pick up and drop out voltage on NEMA Contactors/ Starter coils?
Issue:
Identifying the coil tolerance of a NEMA starter or contactor coil

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
What is the tolerance range on a NEMA type S device coil

Resolution:
-15% to +10% of nominal per NEMA standards.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings