Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum amperage and voltage rating available for the double throw safety switches and are they available in fusible and non-fusible?
Issue:
Product design features

Product Line:
Double Throw Safety Switches

Resolution:
There are two voltage ratings for double throw safety switches. Some of the switches are rated up to 240 Vac and 250 Vdc and others are rated up to 600 Vac and 600 Vdc.

Below are the amperages available in the fusible and non-fusible versions:
1) The fusible double throw safety switches are available in ampere ratings from 30 to 100 A
2) The non-fusible double throw safety switches are available with ampere ratings from 30 to 600 A

NOTES:
1) Square D/Schneider Electric is no longer offering ANY 400 A double throw safety switches, consider using the 600 A, BUT first verify the physical size will work for the application.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings