Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for a replacement handle on an SE circuit breaker?
Product Line:
Circuit Breakers

Environment:
Applies to SEF and SED type breakers

Resolution:
The handle extension was 48161-009-01, and the roll pin was 24209-10400.
These p
arts for the SE frame breakers are obsolete and no longer available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings