Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is 31041-402-02?
Issue:
What is 31041-402-02?

Product Line:
NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Identification

Resolution:
This was a dual voltage coil 120V or 240V, 60Hz for 8502/8536 Size 00 (Series A), 0, and 1 contactors/starters. This coil is obsolete. Order a 120V coil as 31041-400-42, or a 240V coil as 31041-400-51.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings