Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the float only for the 9037DG and 9038JG float switches?
Issue:
Replacement float for 9037DG and 9038JG float switches

Product Line:
Pressure, Vacuum and Float Switches

Environment:
9037 Float Switches

Resolution:
For standard units with no special forms as follows:
The 9037DG1 through 9037DG3 float is obsolete.
The 9037DG4 through 9037DG8 uses float - 65073-003-51. (Obsolete)
The 9038JG1 through 9037JG5 uses float - 65073-003-51.(Obsolete)
The 9038JG7 through 9038JG8 uses (2) floats - 65073-003-51.(Obsolete)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings