Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Powerpact H and J frame breakers be mounted on DIN rail?

Issue:
What is the DIN rail mounting kit for Powerpact H and J frame breakers?

Product Line:
Molded Case Circuit Breaker

Resolution:
Yes, Powerpact H & J frame 3 pole breakers can be DIN rail mounted. Use kit # S29305.
The DIN rail mounting kit requires 15 mm depth on a 35 mm DIN rail.
It fits 3 pole module breakers only. 2p HD and HG breakers will not work with it, and there is no kit for those breakers.

See instruction bulletin, 48940-239-01.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings