Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What catalog number ground bar does the new ``NQ``, 84 circuit panel use? How many are required?
Issue:
What is the part number of the ground bar for the new 84-circuit NQ panelboard? How many ground bar required?

Product Line:
NQ Panelboards

Environment:
Product Features

Resolution:
The new NQ panels use a PK27GTA or PK27GTAL ground bar. Each enclosure is drilled to accept up to 4 ground bars, so up to 4 ground bars can be used in each enclosure.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings