Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will a Zelio RUMF with 230V coil work if supplied with 208V?
Issue:
What are the limits for the coil voltage of 230V on Zelio RUMF relays?
Product Line:
Relays and Timers

Environment:
General Purpose Relays

Resolution:
Yes. Operating voltage limits of RUMF relay with 230V coil are 184V minimum and 253V maximum.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings