Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Class 2601 Reversing Drum Switches available in NEMA 3R enclosures?
Issue:
Can we get a 2601 reversing in a NEMA 3R enclosure

Product Line:
2601 reversing drum switches

Environment:
Products sold and used in the United States

Resolution:
Yes but only for lower horsepower applications, refer to the current Digest for selection. If NEMA 3R is not available for the required horsepower the NEMA 4 enclosed device will be suitable for some 3R applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings