Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a cover with a door be ordered separately for use with the QO612L100S?
Issue:
QO612L100S has no door with the cover.

Product line:
QO load centers

Cause:
Application

Resolution:
Yes it can, but it would require ordering a replacement cover with door and the labeling is NOT supplied with any of the replacement covers. Also, the cost of the replacement cover may exceed or be close to a complete new load center of this same size (like the QO612L100DS). One might consider purchasing a complete load center that comes with a door part of the cover and use the cover on with the existing load center if already installed.

The the cover with door catalog number for load center Series G1, G3, or G4 is: 4055345351.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings