Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On a 8536SCx starter, what is the part number for the housing that holds the contact carrier and coil?
Issue:
Part number for the housing that holds the contact carrier and coil on a 8536SCx starter

Product Line:
NEMA Type S Motor Starters (8536 8736 8606)

Environment:
NEMA Starters

Resolution:
It is called the Power Plant and the part number is 31041-011-52.

NOTE: This does not include the armature, magnet or coil

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings