Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 9065 Solid State Overloads UL listed? What is the UL file number for the standard 9065 Motor Logic type?
Issue:
9065 Solid State Overloads UL Information

Product Line:
Contactors and Starters

Environment:
9065 Motor Logic Solid-State Overload Relays

Resolution:
Yes, the UL file number is: NKCR.E14839.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings