Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the lugs on the LA or LH frame breaker approved for use with finely stranded wire?

Issue:
Fine stranded wire or DLO cable on LA/LH frame circuit breaker lugs

Product Line:
Molded Case Circuit Breakers

Resolution:
No, the lugs are not approved for use with fine stranded wire. Only class B or C cable is approved for use in the lugs, and fine stranded wire is not class B or C. This include ferrules/sleeves/copper shims, which can break and create a false torque reading, leading to a loose connection that can cause arcing/overheating.

NOTE: Finely stranded wire is also referred to as welder's cable or DLO diesel locomotive cable.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings