Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will an FAP circuit breaker fit into an FA enclosure?
Issue:
Product design

Product Line:
Molded Case Circuit Breaker Enclosures

Resolution:
The FAP breakers are NOT listed in the UL procedures to be used in the FA enclosures. They would physically fit, but the FA100_ series of enclosures are marked for lug-lug type circuit breakers ONLY (lugs on both the ON and OFF ends). These breakers would have an L as the third digit of the catalog number prefix (FAL, FHL, etc).

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings