Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an option for non compensated bimetalic overloads on NEMA type S Starters?
Issue:
Identifying available overload relay options

Product Line:
NEMA Contactors and Starters

Environment:
NEMA Type S Starters

Cause:
Product Selection

Resolution:
Non-compensated bimetal overload relays are no longer available in the NEMA product line.

For size 00, 0, and 1 starters a form E can be used to order the starter with an adapter so that it can utilize the IEC TeSys D line ambient compensated overload relays.
For size 2 and above melting alloy and solid state overload relays are the only available direct mount options.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings