Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the standard size of MCC horizontal Bus
Issue:
Standard size of MCC horizontal Bus

Product Line:
Motor Control Center

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
Bus bar size is .25`` x 1.5`` . Note there will be multiple laminations of this depending on the bus amp rating.


CTA-ID : 2049508

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings