Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for Model 5 200 A fuse clip?
Issue:
Model 5 200A fuse clip part number.

Product Line:
Motor Control Center

Environment:
Model 5 MCC

Cause:
Repair parts, maintenance

Resolution:
Part number will be 40555-127-50 and will need a quantity of 6 , Same clip is used for Class H, J and R, if class R you will need a HRK-1020 quantity 1 refection pin. This will be used on a starter or branch.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings