Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the neutral bar on an NQ panelboard made of copper?
Issue:
Neutral bar material on an NQ panelboard

Product Line:
NQ panelboards sold and supported in the USA.

Environment:
Product Features

Cause:
Selection

Resolution:
No, the neutral bar is aluminum. A field installable 100% copper neutral bar is available.
Order kit NQN1CU for .100A, NQN2CU for 225A, NQN6CU for 400A and 600A panelboards

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings