Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for a 200% neutral assembly for the J250S, J250F, J250R, J250DS, J250SS, and J250AWK circuit breaker enclosures?
Issue:
Product design featurs

Product Line:
Circuit Breaker Enclosure

Resolution:
For a 200% neutral application, use the solid neutral SN400LA and use copper wire ONLY.
The SN400LA will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 Kcmil Al/Cu conductors IN and OUT.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings