Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Key Interlocks(KI) be provided on the Circuit Breaker Enclosures used for the Molded Case Breakers (For example the J205S, M800R or P1200AWK circuit breaker enclosures)?
Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Resolution:
KI = Key Interlock
MCB = Molded Case Breaker
CBE = Circuit Breaker Enclosure


NOTES:
1) The actual KI accessory itself for the MCB CANNOT be added to the circuit breaker and used inside ANY of the Square D enclosures.
2) The KI that can be provided on the CBE MUST be factory installed ONLY, there are NO Field installed KI options. See below for the enclosures.
3) Key Interlocks CANNOT be added to the NEMA 1, 3R, 7 or 9 enclosures


The Factory ONLY option that can be added to current certain CBE's are shown below.
For the Legacy L-Frame enclosures, the LA400DS and LA400AWK are the ONLY two enclosures the KI can be factory added.
For the Powerpact B-Frame enclosures, the B125DS, B125A and B125AWK are the ONLY three enclosures the KI can be factory added.
For the Powerpact J-Frame enclosures, the J250DS, J250SS and J250AWK are the ONLY three enclosures the KI can be factory added.
For the Powerpact L-Frame enclosures, the L600AWK and L600AWKMC(this would include the suffix 'VW') are the ONLY two enclosures the KI can be factory added.
For the Powerpact M-Frame enclosures, the M800DS, M800SS and M800AWK are the ONLY three enclosures the KI can be factory added.
For the Powerpact P-Frame enclosures, the P1200AWK is the ONLY enclosure the KI can be factory added.

Additional Notes:
See Section 3 of the Supplemental and Obsolescence Digest 177 for additional information.
For quoting purposes, the enclosure catalog numbers with the suffix KI (examples: J250AWKKI, or P1200AWKKI) should be loaded in the system. If the number is not loaded, add the suffix "KI" to the enclosure catalog number and the KI price adder PER lock must be added to the list price of the enclosure.
For ordering purposes, the enclosure catalog number with the suffix 'KI' can be ordered and ALL circuit breakers and enclosure accessories(solid neutral, ground etc.) should be ordered separately for field installation
For questions contact the Lexington PSG(email = lexpsg@schneider-electric.com).

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings