Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When using a NQMB4LA main breaker adapter kit with an LAL36400 breaker, does the customer have to remove lugs to mount the breaker?
Issue:
NQMB4LA main breaker adapter kit with an LAL36400 breaker, lugs needs to be removed to mount the breaker

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes. The NQMB4LA has busbar connections, so breaker lugs must be removed to install the main breaker.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings