Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the screws come with the NQ deadfront trim kits?
Issue:
Screws or hardware included with the NQ deadfront trim kits

Product Line:
NQ Panelboards.

Environment:
Products sold in North America

Cause:
Product features

Resolution:
Yes, the Hardware bag part number 80122-272-50 comes with the Trims and contains the following :
Information and Installation manual, Torque Labels, circuit numbering strips.
NOTE : A Neutral Bonding strap is not included.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings