Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the current density of standard bus for HVL switchgear?
Issue:
Current density of the bus in HVL switchgear

Product Line:
HVL switchgear

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
600A Aluminum Bus 1/4`` x 2.5`` 960A per sq inch
600A Copper Bus 1/4`` x 2`` 1200A per sq inch
1200A Copper Bus Two - 1/4`` x 3`` 800A per sq inch

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings