Issue:
Which terminal pad kits (RLTB, RLTB4, RL3TB, or RL3TB4) are included with the breaker?
Product Line:
PowerPact R frame breakers
Resolution:
The terminal pad kit RLTB/RLTB4 is supplied for both ends with 2500 A, 100% rated breakers. The terminal pad kit RL3TB/RL3TB4 is supplied for both ends with 3000 A, 80% and 100% rated breakers.
Use suffix YS to omit these terminal pad kits from the breaker, if required, for the assembly plants and for replacement breakers.
You must order the RLTB/RLTB4 terminal pad kits for all other unit mounted PowerPact R frame breakers. Remember to order the appropriate number of AL2500RK lugs for the number of cables being used for the breakers. Each kit contains 2 lugs.
Which terminal pad kits (RLTB, RLTB4, RL3TB, or RL3TB4) are included with the breaker?
Product Line:
PowerPact R frame breakers
Resolution:
The terminal pad kit RLTB/RLTB4 is supplied for both ends with 2500 A, 100% rated breakers. The terminal pad kit RL3TB/RL3TB4 is supplied for both ends with 3000 A, 80% and 100% rated breakers.
Use suffix YS to omit these terminal pad kits from the breaker, if required, for the assembly plants and for replacement breakers.
You must order the RLTB/RLTB4 terminal pad kits for all other unit mounted PowerPact R frame breakers. Remember to order the appropriate number of AL2500RK lugs for the number of cables being used for the breakers. Each kit contains 2 lugs.
Released for: Schneider Electric Canada