Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you replace the contactor in an 8536SC starter?
Issue:
Replacement contactor needed for NEMA size 1 starter

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Replacement contactor needed

Resolution:
Yes. With 120v coils these would be 8502SCO1V02S for 2 poles, 8502SCO2V02S for 3 poles, and 8502SCO3V02S for 4 poles.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings