How can we help you today?

Can the circuit breaker handle, when used in a LA400LS circuit breaker enclosure, be padlocked in the ON or OFF position?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosure

Resolution:
The circuit breaker handle can be padlocked in the ON or OFF position via an integral padlock provision located on the enclosure cover.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: