Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use one AC contactor to run multiple motors at one time?
Issue:
Is it possible to use one contactor to run multiple motors?

Product Line:
Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Using one contactor for multiple motors

Resolution:

Yes, provide separate overloads for each motor and size the contactor according to total Hp and FLA of all the motors added together.
PLEASE NOTE: This is allowed by the NEC only under specific circumstances. Also, we will not provide equipment with multiple overloads due to UL listing requirements.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings