Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does a 2510FG71 operate?

Issue:

2510 Manual Starter Wiring with HOA switch

Product Line:
2510 Type F Manual Starter

Environment:

NEMA Contactors and Starters

Resolution:
When the HOA (cam switch) is in the Automatic mode the external device (thermostat, pressure switch, etc). controls the motor. The contact of the external device must be rated to carry the motor current.

When the HOA is in Hand or Off, the automatic 2-wire control device is overridden.

Refer to below wiring diagram:

2510FG71 Wiring diagram

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings