Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do NEMA contactors and starters come with auxiliary contacts?
Issue:
Determing if NEMA contactors and starters include any auxiliary contacts

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Determing number of auxiliary contacts needed

Resolution:
The 8502S and 8536S come with 1 NO contact as standard.


To add additional contacts please see part number table below for selection:
For Use WithKit descriptionOrdering Information
TypeNEMA SizeClass 9999
Type
External - Field Convertible
SA-SJ00-71 N.O. contactSX6
1 N.C. contactSX7
1 N.O. and 1 N.C. isolated contactsSX8
1 N.O. overlapping contactSX9 *
1 N.C. overlapping contact SX10 *
External - Non-Convertible
SA-SJ00-71 N.O. ContactSX13
1 N.C. ContactSX14
1 N.O. and 1 N.C. isolated contactsSX15
1 N.O. overlapping contactSX16 *
1 N.C. overlapping contact SX17 *
Internal - Non-Convertible
SA-SD00-21 N.O. ContactSX11 #
1 N.C. ContactSX12 #

* - Types SX9 and SX10 or types SX16 and SX17 must be used together and mounted on the same side of the contactor. They are suitable for applications where it is necessary for a normally open contact to overlap a normally closed contact.
# - Types SX11 and SX12 are not for use on NEMA size 3 or larger. Internal contacts can also be used on Class 2510 types M and T manual starters

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings