Product Line:
Tesys F line Contactors and Accessories
Resolution:
First, the LA9 shrouds do not work with the DZ type lugs. They work with compression type lugs such as large ring tongue terminals. When the compression lugs are bolted to the contactor terminals, the threaded portion of the bolt facing the front of the contactor provides a threaded area for the shroud to attach to. The plastic shroud is secured by the bolt threads, and covers and insulates the compression terminal.
Tesys F line Contactors and Accessories
Resolution:
First, the LA9 shrouds do not work with the DZ type lugs. They work with compression type lugs such as large ring tongue terminals. When the compression lugs are bolted to the contactor terminals, the threaded portion of the bolt facing the front of the contactor provides a threaded area for the shroud to attach to. The plastic shroud is secured by the bolt threads, and covers and insulates the compression terminal.
Released for: Schneider Electric Canada