Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can there be top entry or top exit on NEMA 3R HVL/cc switchgear. This is for an OEM account.
Issue:
Top entry or top exit on NEMA 3R HVL/cc Switchgear

Product Line:
HVL Switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No, there cannot be TOP entry or top exit on NEMA 3R HVL/cc switchgear.

The options to resolve this are rear entry/exit with the use of optional rear extensions.

Also, Side entry or exit can be done with the addition of an incoming/outgoing terminal chamber.

The roof design of the N3R HVL/cc is not compatible with entering conduits. In addition, the conduits would enter directly over the switch terminals. The HVL/cc has reduced clearances and should not have any moisture dropping down on top of the switch.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings