Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for MCC5 black plastic control station plates ?
Issue:
black plastic control station plates for MCC5

Product Line:
Motor Control Centers

Environment:
MCC5

Resolution:
Use a 80420-007-01 for the 22mm operators ( 5 operators max) or a 80420-007-02 for 30mm ( 3 operators max) .

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings