Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the degree of protection for the XB5 and XB4 pushbutton products?
Issue:
Identify the IP degree of the XB5 and  XB4 pushbuttons

Product Line:
Push Button and Operator Interface

Environment:
22 mm Push Button

Resolution:
IP66 and IP69K for Selector Switches and multiple-headed pushbuttons. Nema 1, 2, 3, 4, 4X, 12, and 13 unless otherwise stated.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings