Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to backfeed or bottom feed a D-line contactor? In other words, can the line wiring be connected to the bottom terminals, and the load connected to the top?
Issue:
Can you wire the line into the bottom, and load into the top, of a tesys d-line contactor?
Product Line:
Tesys D line contactors

Environment:
Products sold and used in the United States

Cause:
Identifying acceptable wiring practices

Resolution:

No. D-Line contactors are labeled L1 L2 L3 for the Line conductors, and T1 T2 T3 for the load conductors. They must be wired that way to comply with the listed rating. Per code, L1L2 L3 / T1 T2 T3 marked contactors are top fed only.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings