Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the ELM module work on a 2 pole breaker?
Issue:
2 Pole Application for ELM Module

Product Line:
Circuit Breakers

Environment:
ELM Module

Resolution:
It is designed for use with a 3 pole breaker module. It will work with 2 live poles or 1 pole and a neutral.
NOTE: It will not fit on the 2 pole breaker modules (HD and HG 2p breakers).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings