What is the difference between the QO1DM10020TRBR, QO1DM10030TRBR, and QO1DM10050TRBR generator panels?
Issue:
Difference of QO1DM10020TRBR, QO1DM10030TRBR, QO1DM10050TRBR Generator Panels.
Product Line:
Load Center
Resolution:
The difference between these catalog numbers is the amperage rating of the generator fed breaker (20 A, 30 A, and 50 A, respectively) that interlocks with the 100 A utility fed breaker and the receptacle size/configuration, which is appropriate to the given amperage of generator fed breaker used.
Difference of QO1DM10020TRBR, QO1DM10030TRBR, QO1DM10050TRBR Generator Panels.
Product Line:
Load Center
Resolution:
The difference between these catalog numbers is the amperage rating of the generator fed breaker (20 A, 30 A, and 50 A, respectively) that interlocks with the 100 A utility fed breaker and the receptacle size/configuration, which is appropriate to the given amperage of generator fed breaker used.
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.