Can the shunt trip on an LX breaker be field replaced?
Issue:
Is the LX breaker shunt trip field replaceable?
Product Line:
Molded Case Circuit Breakers
Resolution:
Yes. The only available part number is LC11021 which is a 120-240 Vac shunt trip. The rest are obsolete.
Is the LX breaker shunt trip field replaceable?
Product Line:
Molded Case Circuit Breakers
Resolution:
Yes. The only available part number is LC11021 which is a 120-240 Vac shunt trip. The rest are obsolete.
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.