Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What size power fuse clips are used on a size 3 combo starter unit with fusible disconnect?
Issue:
Fuse clips for Nema size 3 Combo Starter

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8538 Combination Starters

Resolution:
100A fuse clips.
Class R fuse block assembly is part # 80420-850-55.
Class H fuse block assembly is part # 80420-850-52.
Class J fuse block is part # 80420-851-52.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings